This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需要设计一个正负可调的电源,输入直流36V,输出为正负30V左右可调,
目前的问题为能否将两个LM2596芯片输出串联共地的方式达到设计目的,输出三端分别为正负和地,
二者输出串联的话,两个芯片可以输入可以连一起吗,或者有什么别的芯片可以推荐
负载电流2A,不是用变压器输出,用两个2596芯片分别做正负压的可调输出,不确定这个方案是否可行,因为我看到2596输出正电压是符合我的需求的,但对于使用2596输出可调负电压还是有些疑问
Hi
正压可以,负压不行,负压需要输入电压大于66V(30+36V)的降压芯片,电流能力大于2/(1-30/66)=3.7A.
HI
如上,按照上面条件选择合适的降压芯片是可以做到负压输出的。
如果直接给负压,你需要确认这个负压源的电流能力,就像上面选择合适的降压芯片但是必须有足够的电流能力一样。