This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2592是一款固定频率为150KHz的最大输出为2A的DC/DC,是NS比较老的芯片,目前市面上有很多国产通用料。
1.由于输出电流很小50-80mA,所以LM2592会工作在DCM(非连续模式)模式,进入断续模式后,当输出电流不断减小时,开关管的导通时间也会不断减小,当减小到一定时候就会进行降频。输入电压的升高会增大电感的上升速度,所以相同输出电流,输入电压越高导通时间越短,这种降频是为了提高系统的效率,没有关系。
2.您的问题可以确定是在轻载的时候输出摆幅很大,这个首先确认PCB-Layout没有大的问题,输入电容,芯片,二极管组成的环路尽量小;其次就是可以尝试把电感和输出电容加大,输出电容选择ESR较小的电容,并列1~2个16v/10uF的陶瓷电容;;最后如果系统电流只有80mA,建议采用0.5A甚至更小电流的DC/DC来设计,这样可以选择更小饱和电流的电感,更小电容,以便降低成本。
3.如果后续有设计可以参考NS更新的Simple Switcher LM2267X和LM557X系列,从0.5A-5A,频率从200KHz-1MHz可调。
从波形上来看,电压加大,占空比变小,由于其工作在断续状态,所以后面会有一个衰减的振荡产生。但是一个问题是第二张图看起来频率在抖动,不正常。图的后面还有一个18U,建议去掉在看看,有可能频率抖动导致5V不稳。或者把L2减小到30uH试试。