This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于国半的LM2592电源芯片问题



TI技术支持:
     你好!我们的应用中大量采用了贵公司的一款DC-DC电源芯片——LM2592HVS,但在产品大量出货后发现该电源芯片输出5V电压不稳定,进一步导致单片机等电路损坏;
(我们的应用电路是:LM2592输入电压为50V,输出5V,平均消耗电流50mA,最大消耗电流80mA,环境温度在50~60℃)
 
 
我们通过示波器等多种方法分析发现该器件在输入电压为12V,其开关频率如下
 
而在输入电压变大到30~50V时,其开关频率就突变了
        
 刚开始我们还一直以为是LM2592的批次,但我通过不同渠道采购原厂的不同批次的KM02**\JM96**该款器件,也都存在开关频率不固定的现象,另外我也更换过输出端的肖特基二极管(SS26\CMSH100)和电感(100uH)也都没有改善;不知你们的工程师是否有遇到类似的问题,希望你们能协助我分析和处理该问题。合作愉快!
  • 你好:

         负载电流是多少?建议将电感L1、电阻R21去掉,再重新做测试。

    数据手册中第3页:Note 6: The switching frequency is reduced when the second stage current limit is activated. The

    amount of reduction is determined by the severity of curren overload.

  • Trevor 你好,

     我的设计电路负载电流最大80mA @ 5V,我尝试去掉L1和R21,还是老样子,请麻烦您再帮我解答一下,

    你们那边是否有硬件条件 或者 官方的DEMO评估板进行验证一下

  • LM2592该器件是固定频率150kHz的pwm,不应该会出现这种想象的,

    我测试过其他固定频率的DC-DC器件,并且调高输入端的电压,测量的结果开关频率就是固定的,只会改变脉宽的占空比

  • 电感的选择是最关键的,还有就是输入端的退耦大电容和输出端滤波电容

  • LM2592是一款固定频率为150KHz的最大输出为2A的DC/DC,是NS比较老的芯片,目前市面上有很多国产通用料。

    1.由于输出电流很小50-80mA,所以LM2592会工作在DCM(非连续模式)模式,进入断续模式后,当输出电流不断减小时,开关管的导通时间也会不断减小,当减小到一定时候就会进行降频。输入电压的升高会增大电感的上升速度,所以相同输出电流,输入电压越高导通时间越短,这种降频是为了提高系统的效率,没有关系。

    2.您的问题可以确定是在轻载的时候输出摆幅很大,这个首先确认PCB-Layout没有大的问题,输入电容,芯片,二极管组成的环路尽量小;其次就是可以尝试把电感和输出电容加大,输出电容选择ESR较小的电容,并列1~2个16v/10uF的陶瓷电容;;最后如果系统电流只有80mA,建议采用0.5A甚至更小电流的DC/DC来设计,这样可以选择更小饱和电流的电感,更小电容,以便降低成本。

    3.如果后续有设计可以参考NS更新的Simple Switcher LM2267X和LM557X系列,从0.5A-5A,频率从200KHz-1MHz可调。

  • 从波形上来看,电压加大,占空比变小,由于其工作在断续状态,所以后面会有一个衰减的振荡产生。但是一个问题是第二张图看起来频率在抖动,不正常。图的后面还有一个18U,建议去掉在看看,有可能频率抖动导致5V不稳。或者把L2减小到30uH试试。