This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求锂电池升压方案

Other Parts Discussed in Thread: TPA6120A2, TPS65130, BQ24253, BQ24090, BQ24133

需要设计一款便携式耳放,耳放IC希望使用TPA6120A2,但是这个IC工作电压在+-5——+-15V。充电部分使用通用的USB 5V 充电

第一个备选方案是 使用一节锂电池3.7V需要加一个负压IC,并且需要做升压。这个方案的话有什么IC可以推荐呢。

第二个备选方案是使用两块锂电池,但是充电的方案可以用那个呢?

另外我之前使用TPA6120做的USB耳放,使用电脑的USB供电,加负电压泵IC,供电是+-5V。结果底噪很大,查看IC资料TPA6120这个IC对电源的抑制只有70几DB。问题:这款IC是不是不适合用USB供电,如果可以用USB供电,可以做些什么处理,使底噪更小呢?

  • 1.推荐TPS65130,可以满足你的5V ->+-15V的转换。

    2.单节锂电池可以使用我们的BQ24090线性充电器,也可以使用效率高些的BQ24253开关充电器。如果直接通过USB充电,建议单节电池。

    3.BQ24133可以独立完成1-3节锂电池的充电工作。

    4.如果要抑制电源纹波,可以在+-电压上添加我们的LDO作为有源滤波器,如

    TPS7A4901(Positive LDO)

    TPS7A3001(Negative LDO)

    谢谢。