This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700方案,IC不启动,无输出电压



按照WEBENCH的设计图,如附件,电源不工作,无输出电压,测量IC的Vdd电压不到2V,将启动电阻改小到3M欧,还是无法启动,D4管换为快恢复管也一样。请协助分析不工作原因,谢谢。

变压器绕组比例:NP:NA:NS=134:37:24,

//注:接220V/50Hz市电,输出电压设计的为16V,辅助绕组电压设置为25V