This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF1933: Failed Solderability test

Part Number: REF1933


Dear,

我们最近检测了REF1933AIDDCT,三个批次DC:2136/ DC:2207/ DC:2247,检测了一共四片样品,可焊性测试的成功率都在95%以下,其中2207的覆盖面是84% &93.75%,DC2247的覆盖面93%,DC2136的覆盖面只有70%。请问这个是正常的吗?

还有DC2207的一片电流测试也没通过,Low Vref output Vref =3.29329V  /  Low Vbias output  Vbias =1.64672V , 这种不良率也是正常的吗?

感恩您的回复~

\

We test 4 pieces, moved 4 pieces to test the output Vref and Vbias voltage.

Found 3 pieces passed that the Vref was within 3.2967V to 3.3033V and the Vbias was within 1.64835V to

1.65165V, but 1 piece failed that the Vref was less than 3.2967V and the Vbias was less than 1.64835V.

Parts Passed XRF, Failed Solderability test.