lm3421 VRCT(RCT脚上电压),在我给定5v输入的时候为1.4v,在14v输入时到了1.99v,不是应该是vin/25的关系吗?还有再问一下over-voltage hysteresis (VHYSO)的含义,我是用weebench设计的。。附原理图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
lm3421 VRCT(RCT脚上电压),在我给定5v输入的时候为1.4v,在14v输入时到了1.99v,不是应该是vin/25的关系吗?还有再问一下over-voltage hysteresis (VHYSO)的含义,我是用weebench设计的。。附原理图
1.你的8脚 nDIM是怎么连的?
2.你的MOS管是如何连的,测量一下MOS栅极的电压,看是否为高电压?
3. 将MOS管的栅极直接连高电平看是什么效果?
谢谢
你好
如果我把LM3421的最大电流设定为600mA,通过调节PWM让输出电流输出为300mA,然后去调节输入电压,这时候输出的电流发生变化,输入电压升高则电流上升,输入电压下降则电流减小(输入电压都在范围内)。这样是正常的吗?