This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教工业仪表电源方案(430单片机、DAC8760、继电器、蜂鸣器)供电。

Other Parts Discussed in Thread: MSP430F5438A, DAC8760, TPS54340, LM2733, LM2588, LM2576

您好!想请教个电源方案。

目前需要供电的:

MSP430F5438A:3.3V

蜂鸣器:用5V。

DAC8760:12V (只需输出0~5V和4~20mA)

继电器:12V。

现场供电通常是12V~24V,但是不排除用12V供电导致电压降低到9V,所以想用个宽压9~36V的方案。

目前已经用TPS54340将电压9~24V转为5V,在用TPS79533生成3.3V。

DAC8760和继电器都需要12V,继电器虽然有5组,但是通常只有2组打开,一个继电器大概70mA以内。

1. 请问有什么12V芯片,因为布线面积不多,电路简单点的, 要求(9~36V输入),+12V输出即可。

2. DAC8760和继电器共用一个电源没什么问题吧?