Other Parts Discussed in Thread: BQ24195, BQ24157S, BQ24157
我的电池是1节锂电池,2000mA左右。
我的模块电源是5V输出,最大输出700mA电流。
1、当模块电源有电的时候,给电池充电。这个时候模块电源是5V,最大700mA,给电池充电需要降压吗?电池一般是3.7V到4.2V
2、当模块模块电源没有电的时候,电池给模块供电,模块工作最大工作电流500mA。这个时候电池给模块供电需要升压吗,因为模块需要5V电压。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你是不是需要做一个类似充电宝东西?即可对电池充电,又可让电池升压输出。
如果是的话,可以考虑bq24195,bq2426x等
1.请问你的系统中有MCU么?
2.外部充电和由电池对外供电这中间有切换时间么?
3.如果希望比较简单,可以使用线性充电器 加 boost + oring 来设计,可以实现不间断的5V输出。