This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问TI的人,求一个电池的充放电芯片?输出电压是5V输出

Other Parts Discussed in Thread: BQ24195, BQ24157S, BQ24157

我的电池是1节锂电池,2000mA左右。

我的模块电源是5V输出,最大输出700mA电流。

1、当模块电源有电的时候,给电池充电。这个时候模块电源是5V,最大700mA,给电池充电需要降压吗?电池一般是3.7V到4.2V

2、当模块模块电源没有电的时候,电池给模块供电,模块工作最大工作电流500mA。这个时候电池给模块供电需要升压吗,因为模块需要5V电压。