This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: 关于电量计阻抗跟踪配置(impedance track configuration)十六种选择(load select * load mode)的差异及影响

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: EV2400

TI 工程师,您好。

我的产品为笔记本,电池设计75wh(3S1P),面密度21.6,内阻32mΩ,选择的IC是BQ40Z50-R1。

我在验证电池FCC时,发现两个问题:

一个是FCC对比实际放电数据偏小,

另一个是电池放电电量在10%~15%左右时会跳变到0%。

修改阻抗跟踪配置,70与31 40会导致计算FCC有较为明显的差异。

1.  如果load select 选择7, load mode 选择0 ,即 default 的Max Avg I last Run , 在电池重载(约0.7~0.8C)放电的下一个循环会显示FCC大约68Wh。电池电量在10%~15%左右偶尔会跳到0%。

2. 如果load select 选择3,load mode 选择1,即AverageCurrent() x average Voltage(),在在电池重载(约0.7~0.8C)放电的下一个循环会显示FCC大约70Wh。电池电量在10%左右偶尔也会跳到0%。

3. 如果load select 选择4,load mode 选择0,即AverageCurrent() x average Voltage(),在在电池重载(约0.7~0.8C)放电的下一个循环会显示FCC大约75Wh。电池电量暂时未发现跳变。

通过EV2400实测,几种设置电池放电实际可以接近75Wh。

       因为样本数量有限,那么想请教一下,选择16种模式中哪个模式可以让FCC更接近真实的75Wh?分别会带来什么负面影响?

除了impedance track configuration外是否还有其他设置可以进行调整优化FCC上报对比实际输出偏小的问题? 以及解决或者缩小电池电量跳变的问题?

还望指导,非常感谢!