This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: 带到满载左右IC异常关机

Part Number: UCC28070


问题描述:带载到满载功率3KW左右时,工作时间大概30S左右后,PFC的驱动停止发波,输出电压下降到输入整流后的电压,开始打嗝周期60ms左右
        分析过程:1.测试IC的管脚电压VAO稳态电压3V左右,远离阈值5V的功率保护点
                      2.测试IC的VSENSE输出电压反馈脚电压3V,远离过压保护点3.1V
                      3.输入电压检测脚VINAC电压2.36V,波形也正常
                      4.IMO脚的电阻通过官方计算表格计算的,实际经过多次调试分别尝试27K 30K 39K 无效果
                      5.电流检测脚 CSA/CSB电压1.3V,设置过流保护点的电压3.5V
                      6.软起SS脚电压稳态时高电平,IC驱动停止后,SS正常下降(排除SS被拉低,已断开SS外接的电路)
                      7.VCC测试是稳定的电压12V
                      8.RYSNTH引脚电压未达到5V,尝试加大电阻到几百K无效果,计算值150K左右
                      8.把输出电压从410V调到390V之后再次测试发现依旧功率达到3KW左右时保护(结合测试的现象以及IC管脚电压,像是触发过功率保护一样)
测试的波形都是有比较大的毛刺,观察中心值均为达到保护阈值,另外所有的波形在保护前后没有明显的变化。
  (4)原理图:参考TI官网推荐电路,IC外围参数基本也是计算表格计算得来