我不需要USB充电协议,不需要OTG功能,我用12V的适配器输入
1,请问我可以把下图输入电路中这部分去掉吗?
2,然后在VBUS输入前端接一个TVS管可以吗?
3,可以的话我后端系统(mcu)的供电全部由SYS提供可以吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我不需要USB充电协议,不需要OTG功能,我用12V的适配器输入
1,请问我可以把下图输入电路中这部分去掉吗?
2,然后在VBUS输入前端接一个TVS管可以吗?
3,可以的话我后端系统(mcu)的供电全部由SYS提供可以吗
谢谢!
1,那我是不是可以把图中的上拉的OTG脚,直接接地,手册上说OTG是USB电流限制和升压使能,我不使用PMID的输出那么我就可以给OTG接地关闭升压?
2,sys的输出电流最大能达到多少? 我后端用到的是几个上拉,然后驱动一个双色led指示灯,然后一个TL431的2.5V基准原
1,那我是不是可以把图中的上拉的OTG脚,直接接地,手册上说OTG是USB电流限制和升压使能,我不使用PMID的输出那么我就可以给OTG接地关闭升压?
不使用升压,可以将OTG接地
2 sys的输出电流最大能达到多少? 我后端用到的是几个上拉,然后驱���一个双色led指示灯,然后一个TL431的2.5V基准原
可以达到几安培的电流。
谢谢