Other Parts Discussed in Thread: UCC28810, TL431, UC3844
新手用UCC28810做了一个恒压源,反馈使用的是TL431,电感56:29:13,电感量1mH,漏感26uH,EE25.4磁芯,后级电容只使用220uF是因为要换成MLCC电容,而且换成1000uF也无法正常启动。
输出电压为30.5V,电流0.189mA
输入电压220V,电流0.0744AA
效率仅为35%,之前用UC3844做差不多也是30%上下,板上无明显发热,使用的是普通的万用表测量的,不知是不是仪器问题。