This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: BQ77915的定义和充电保护

Part Number: BQ77915

在BQ77915的规格书中,有UV的定义:1.2V~3V. 对于这个定义,我有几个问题:

 

  1. 1.2V~3V是不是一个UV区间?还是要预先设定某一个阈值做为UV的一个界限?比如设定2.5V,高于2.5V就不是UV,低于2.5V就是UV.

 

  1. 如何UV是一个区间1.2V~3V. 那么在这个区间内,就只能预充电,而低于1.2V,就认为电池死了,不能再充电了?

 

  1. 在一个4串的电池中,是不是有一个电池处于UV,BQ77915就会阻止电池组继续放电?

 

  1. 在一个4串的电池包处于shutdown的模式中,BQ77915为中心的BMS会消耗电池包多少电流? 如果以电芯2500mAh,自放电为零为例,可以放多长时间,直到电芯低于UV-1.2V. 或者有没有什么计算方法或者公式?

 

  1. 在预充电期间,会有均衡充电的功能吗?

 

  1. 在一个4串的电池包中,有一个电芯低于UV-1.2V,是不是这个电芯就不能预充电了?
x 出现错误。请重试或与管理员联系。