你好!
我在一个项目中使用了TPS2543这款芯片制作一个USB充电的接口,由于要求在充电的时候能够进行USB通信,所以选择了其CDP模式进行工作,根据资料来看,在这中模式下能达到1.5A的充电电流。但是在测试中,给三星的S4充电的候怎么实验都达不到1A以上,最多900mA,请问一下,有没有什么好的技术建议呢??谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
我在一个项目中使用了TPS2543这款芯片制作一个USB充电的接口,由于要求在充电的时候能够进行USB通信,所以选择了其CDP模式进行工作,根据资料来看,在这中模式下能达到1.5A的充电电流。但是在测试中,给三星的S4充电的候怎么实验都达不到1A以上,最多900mA,请问一下,有没有什么好的技术建议呢??谢谢!
Hi Kang Zhang,
1.请问充电源是什么?是插在笔记本上用现成的USB口还是使用电源供电?
有可能笔记本端本身存在限流操作。先保证笔记本USB口有能力带载1.5A
2. 请问此时的VBUS电压是多少?
VBUS电压加上线损,如果低于5V或者更多,是可能会出现充电限流。
谢谢。
你好!谢谢你对我回答!
1、充电电源是用一个DC/DC的芯片,可以输出2.5A,所以这里可以肯定电源处没有限制。
2、嗯,我们的仪器检测出USB线中间的电压为4.8V,电流为900mA,而TPS2543的输出端是5.1V。
3、目前主要是给三星S4手机充电
HI,FAE 你好,我在做车载DVD方案,用的TPS2543,也用的是CDP模式,16.9k与80.6k的限流电阻,DCDC输出可以到3A,我把USB输出提高到了5.3v,而且也是根据你们的参考设计做的原理图,可是测试苹果5S与小米3最多到1A,怎么也到不了5A,不知道为什么?
Nicky,
首先,小米和iphone5s默认的适配器的充电电流都是1A,正常情况下充电电流都是1A。小米3提供快充适配器,支持2A充电电流,但是分英伟达和高通版,情况可能会不一样,因为使用的充电方案应该是不一样的。
Iphone5s在网上没看到能够使用更高电流进行充电的情况。
所以您需要看手机是否支持CDP模式下的1.5A,有可能手机本身在设计的时候输入电流就限制在了1A,无论DCP或CDP。这种情况下,除非修改手机固件的充电寄存器设置,不然,光靠供电端进行改动并没有作用。
小米3有人用2A其他品牌适配器,做到2A充电。
您可以试试DCP模式下充电电流多少。
Thanks.