This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

学习与理解UC3842满载工作的疑问



如上是电原理图和满载次级二极管波形图
DS波形能看出来是工作--停止--工作这样的循环
这样是为什么?
怎么解决呢?

ps 
变压器 1mH  90:9:18:12  (pri:sec12:sec24:bis16) 
MOS管下面的限流电阻1.25ohm

输入直流200~300V 

以上是他人问的问题,连接地址是:http://www.deyisupport.com/question_answer/analog/power_management/f/24/t/73113.aspx

针对上列的问题:Frank 1 作出了另一种817的接接方式,且好几位工程师都出具了相应的参数。

其实针对个人来说,817只应用了那么一种而已,能学会这点问题点也是一件不错的好事情。