This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563201: 示波器测量到的纹波电压很大。输出5V,纹波达到200mV, 什么原因造成的?还是我的测量方法不对?

Part Number: TPS563201


电路原理图如下,器件参数按照datasheet中的5V输出推荐的配置。

PCB布局如下,C65放在背面。

示波器使用 RIGOL:DS4014E (4Channel 100Mhz 2GSa/s);

测试方法:

1.  使用无源探头,X1衰减、DC耦合、1Mhz输入阻抗,测量C65两端的电压,空载时电压最大值约为5.241V,最小值约为5.025V,截图如下:

2.  使用无源探头,X1衰减、AC耦合、1Mhz输入阻抗,测量C65两端的电压,空载时电压最大值约为100mV,最小值约为-110mV。

这样的波动正常吗?还是我的测试方法有问题?

  • HI

         输入电容调小,建议10uF以上。

         输出电容建议2个10uF并联降低输出电容ESR.

         Layout建议你尽量参考datasheet, 同时测试上有些不对,你可以参考datasheet上波形的测量,拉开一些,800ns/div.