This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LNK306+TPS560200输出不正常

Other Parts Discussed in Thread: TPS560200

我用LNK306和TPS560200从AC220V得到DC12V和3.3V,电路图如下所示,VCC输出13V左右,VDD是4.5V,带不带负载都一样,另外在C4上并100uF电解电容,R3上并20pF或者470pF电容时VDD是3.9V,没有隔离不方便测试。主要是后面的TPS560200不正常,理论上应该是3.3V输出,不知道哪里有问题?