选用上图电阻,在5A的时候也没关闭输出这是为什么呢?是我设置错误还是我理解错PDF了,请各位前辈指点下,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢你的回复!我列出计算过程请帮我看下有没有错,谢谢:
输入10-34V,输出8.4V,7A,220KHZ
Ton = (8.4V/12V)/220 kHz = 3181.8 ns //是最大值还是最小值,还是其他什么?
△IL=(12-8.4)*3181.8us / 15uh=763.623 //算出来的值是这样,单位转换不知道该怎么转.根据PDF实例估算应该是7.63623
ICL=7A - 7.63623/2=3.181885
RLIM=3.181885*3.3mΩ / 75 x 10-6 =140R
请帮我看看,计算中是否存在错误,谢谢。
----------------------------------------------------------------------
由于没有140R电阻用的是150R的,但是在10A电流输出的时候也没反应,在限流保护开启的时候是打嗝输出还是什么?