Other Parts Discussed in Thread: TPS23731, TPS23751, TPS23754
1.What is the function of inductance L3 and is it necessary?

2.What is the function of CL1?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
1, 必须的,正激的电路配置(类似buck电路功能上的电感)。
2. CL1用于短路,就是不用到B1100.
Yes,It's made into a flyback type.Please help confirm if there are any issues with the current design first.
Are there significant differences in efficiency between these two schemes?Because the customer has specified a solution, it is currently uncertain whether to change the solution.