This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: LM5116 设计5.2A 24V输出 带负载 5A,电源上电启不来问题

Part Number: LM5116


根据TI官网下载的LM5116_quickstart表格计算得出以下参数

Vout (V)    24

Vin(min)(V)    36

Vin(max) (V)  51

Maximum Ave Load Current (A)    5.2

Ripple Current% of Maximum Load Current   30%

VCCX voltage (V)   0

Recommended IC  LM5116

Target(% beyond Max load)   20%

Average Load Current at Current Limit(A)  6.24

Short Circuit Current (A)  9.2

Current Sense Method   R-sense

Low-side MOSFET Rds (mOhm)    16

Rs (mOhm)  12.0

Fsw (KHz)  250

Rt (K Ohm)  12.50

Cout1 (uF) 220      实际用  EEHZK1V221UV    220UF/35V  松下

Cout2    (uF)    44       实际用  22uF/35V  *2    

Cout (uF)  262

Capacitor ESR (Ohm)  0.08

Vout (mV)  124.8

L (uH)  32.6      实际用33UH  9A   1350封装

Camp (pF)   907     实际用1nF 

Rramp (KOhm)  126.7    实际用127K

Required?   Yes

Vin Umder voltage Thres hold (V)  25

Ruv2 (KOhm) 210.0

Ruv1 (KOhm) 10.27     实际用10K

Cft (uF)  1.00

toff (ms) 7.00

ton (ms) 1.02

Duty Cycle  12.7%

Rfb1 (Ohm)  1210           实际用12.1K

Rfb2 (Ohm)  226.91        实际用22.6K

Required ?  NO

Redm (Ohm)  1861        实际用1.87K

Low-side MOSFET Qg at VGS =4.5 (nC)   20.0

Low-side MOSFET Qg at VGS =10(nC)   25.0

Cvcc (uF)  0.45     实际用 1uF

Hi-side MOSFET Qg at VGS =4.5 (nC)   20.0

Hi-side MOSFET Qg at VGS =10 (nC)   25.0

Chb (uF)  0.23      实际用470nF

VCC Start-Up Current ICC (mA)  12.3

VCC Run Current ICC (mA)  12.3

Cin (uF)   12.5     实际用4.7uF*4 +0.1uF

Bandwidth Fc (KHz)  25.00

Modulator Gm (mod) (A/V)  8.35

Modulator cross over frequency Fc(mod) (KHz)  5.03

Rcomp (KOhm)  112.7     实际用 39K  (采用的是Manual模式 )

Ccomp (pF)  565         实际用1.5nF (采用的是Manual模式)

Chf (pF)  187               实际用15pF  (采用的是Manual模式)

Error Amp Zero (Khz)  2.5

tss (min) (ms)  6.09

tss (ms)  12.1

Css (uF)  0.100      实际用100nF

 

MOSFET    BSC160N10NS3G      VDS  100V      RDS   16mOhm   Id  42A    Qg  19nC    25nC

测试带载  1A  2A 3A 4A   Pk-Pk   40mV -80mA    Apm  20mV

测试带载  5A  6A      Pk-Pk   60mV -100mA    Apm  40mV

问题点,打开负载仪设置 CC模式 电流设置 1-2A    再开电源,电源正常启动

              打开负载仪设置 CC模式 电流设置 3A    再开电源,电源有可能正常启动

              打开负载仪设置 CC模式 电流设置 4A    再开电源,电源有可能正常启动

              打开负载仪设置 CC模式 电流设置5A    再开电源,电源不能正常启动

             打开负载仪设置 CW模式 设置100W    再开电源,电源不能正常启动

请问有什么办法设置,看一下是什么问题,我觉得是上电,就过流保护了。