This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700-Q1: 电源瞬断,BATT会异常抬起

Part Number: LM74700-Q1


您好

当前遇到的问题:12V电源做瞬断实验时,过LM74700后的P-BATT电压会被抬起,然后稳定在2.6V

回路图:

波形:参照蓝线

经分析,异常抬起是由LM74700造成的。

分析方法:使用跳线越过LM74700这个IC,P-BATT不会出现异常抬起电压,稳定掉到0V

还请帮忙确认

1. 什么原因造成电源会被异常抬起?LM74700有什么特殊的功能吗?

2. 如果对LM74700进行仿真,用PSpice for TI吗?有现成的周边回路模型吗?抱歉,PSpice还没会使用