This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65235-1: TPS65235-1: 技术问题

Part Number: TPS65235-1


Hi ti team,

客户在做物料承认测试的时候有几点问题需要确认下:

1、规格书写过流保护最大值为0.688A,但我们实测为1.15A,帮确认是否OK

2、当过流、短路、过温保护时,FAULT脚会拉低,但取消保护后,输出正常,FAULT没有恢复拉高,这点是否OK

3、规格书只管控13V-18V的上升时间,目前测试OK。但我司实际使用的是日本市场场景,用15V,测试了0V-15V上升时间为4.8ms,是否OK

4、截图中的两种恢复FAULT的方法如何实现,实际使用时软件控制还是硬件控制?

  • Hi

        1. 取决于电流保护设置。

        2. 正常,fault跳转条件见datasheet第13页最上面描述。(或者见你提供的截图)

        3.没有具体定义,我这边也没有数据参考。

        4.  上面提到1是硬件,2是软件控制。