This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40Z80 CHG/DSG驱动电流

Part Number: BQ40Z80


现在我这边使用BQ40Z80来设计一块新的BMS板子,充放电MOS回路是各并联5个大功率的MOS管。所以需要了解一下CHG/DSG驱动电流的情况,但我在规格书上没有找到具体的资料。我不确定BQ40Z80的充放电时是否能驱动的了并联5MOS管。需要麻烦帮忙确认一下。谢谢。

MOS管的资料:NTMFS5C410NLT1G

Qg:143nC(Vgs=10V);Rds:0.82mΩ(Vgs=10V)最大值;Vds:40V;I:330A;Vgs(th)=1.2V;Rg:1.0Ω;VON:11.5V