This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542EVM: BQ27541 部分参数更新部分参数是默认值的问题

Part Number: BQ27542EVM

客户反馈几率性的存在部分参数更新,部分参数是默认值,

我们自己从库存的成品中,抽测了20台,发现有2台 FC Set%变成0的情况,

想咨询下,

1.通过GG文件更新参数,是否可能存在部分不成功的情况?客户反馈的是FCC(full charge capacity)没有更新,这个是可能是什么原因造成的?

2.图中FC SET%为0的情况,可能是哪种原因导致的,如何排查?

3.FC SET%为0,对客户正常使用是否有影响?

4.有些参数,比如lifetime/calibration相关的,有变化是正常的吧?

5.GG文件中,哪些参数是静态的,后续不会改变?哪些是动态的,后续可能会自动更新?

6.导入GG文件后,哪些参数我们需要检查,哪些可以忽略不用检查?

  • 您好

    1,如果成功烧录,如果FCC值不会会修改成功。

    2,FC set %0这个不会自动更新为0,建议检查哪些流程会有可能修改到参数。

    3,If set to anything besides –1, the Primary Charge Termination algorithm will not be used and instead the FC bit is set when the SOC reported by the gauge reaches this specified percent through coulomb counting or passed charge current.

    4, lifetime/calibration是变化的参数。

    5,校正相关的参数会自动更新,lifetime和black box也会更新。

    6,设置的参数不会变动,校正的参数会变动。

  • Hi Star,

    谢谢回复,以下问题请帮忙确认下:

    1.black box指的是隐藏的参数吗?

    2.生产只烧录GG文件可以么?对使用会有什么影响吗?

    3.“keep scanning”打开后,是否可能会影响参数的写入,导致参数被误写?

    4.GG文件所有参数对应的相关I2C的协议,有相应的公开文档么?

  • 您好,

    1,black box是记录芯片特殊的保护状态,如果没有请忽略。

    2,建议使用DFFS文件。The DFFS file is used when the original device has the same firmware version.

    3,写入时不建议打开auto refresh

    4,非常抱歉没有找到相关文档。