Part Number: BQ76200
设计了24串锂电池BMS采样系统,但是还要设计MOSFET充放电电路 ,所以使用了之前设计用的BQ76200;
设计完了之后发现BQ76200最大电压100V,因为充电泵电容电压会加14V左右,推荐电压75V ;
但是24串PACK电压100V ,已经超出了额定范围电压,怎么再不替换BQ76200的情况下安全使用BQ76200驱动MOSFET?
求大佬指点!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The BQ76200 has a 100V abs max on the highest pins. Leaving about 16V for the charge pump voltages with variation in operating conditions would put the maximum BAT+ voltage at 84V. You will need some budget for transients on BAT+ and PACK+ also. For lower voltage cells and quiet environments it may work acceptably, but e-bikes are traditionally a noisy environment. Certainly check the system specifications and budget, but the BQ76200 may not be the best choice for a driver.
You might look at isolated gate drivers, see options at http://www.ti.com/gatedrivers . Some designers will design their own gate driver circuit for the voltage, or use low side switching and isolate the communication path.