This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138_FW_SDK: BidirectionDCDCFirmware-1.2 UCD3138 编译问题

Part Number: UCD3138

CCS12 编译 BidirectionDCDCFirmware-1.2 UCD3138出现下列问题,请帮忙解决。谢谢!

"../Dev/Linker Files/cyclone.cmd", line 97: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".stack" size 0x800. Available memory ranges:
STACKS size: 0x190 unused: 0x190 max hole: 0x190
error #10010: errors encountered during linking; "BiDirection_DC-DC_UCD3138.out" not built

x 出现错误。请重试或与管理员联系。