Other Parts Discussed in Thread: UCD3138
CCS12 编译 BidirectionDCDCFirmware-1.2 UCD3138出现下列问题,请帮忙解决。谢谢!
"../Dev/Linker Files/cyclone.cmd", line 97: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".stack" size 0x800. Available memory ranges:
STACKS size: 0x190 unused: 0x190 max hole: 0x190
error #10010: errors encountered during linking; "BiDirection_DC-DC_UCD3138.out" not built