This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV问题求助,急!!!!

Other Parts Discussed in Thread: LM3409HV

我用直流48V输入  四组LM3409HV驱动8窜LED,每组驱动2串LED,  LED的Vf3.45   动态电阻根据计算0.3左右,每串LED 7颗  电流1A 

那么webench设计就是48输入(600W开关电源)   24.15V,2A输出  设计如下:

这样参数默认出来的工作频率是1.006MHZ,为了减少发热我把频率定在400KHZ左右

原理图如下,其中画圈的元件的值都改成webench推荐的了,P-mos用的是webench推荐的SI7465dp

PWM的频率是50K

这样以后出来的电流在带上LED测只有150MA左右,电压也只有将近21V

 VIN VCC之间的电容断电压是典型值6V左右,EN脚的波形是50KHZ的PWM波没错,但是我在与P-MOS相连的PGATE脚抓,但是是有一点点波形,占空比非常低,但是这个波形我的示波器读不出频率

问题现象就是   电流150MA左右,电压21V左右 ,P-GATE频率读不到而且不稳定

(我的led是之前用过的旧的,我也怀疑过是LED性能导致电流上不去,但是我用恒压恒流源测电流是可以到1A的)

请各位给分析分析,比较着急,谢谢了!