This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是我设计的电路,在实际测量时,VFB=1.26V,电源纹波为三角波,VPP=200mV,频率为100K,输出电压为24.9V,输出电压为什么差0.9V,其他电压设计输出都很准,最多相差0.1V
这是什么原因造成的,图中器件都是正常的。而且用官网的电源设计软件,输入48-85V,输出24V,显示不能用LM5013设计,这是怎么回事?
Hi
正常是20mV的纹波,200mV是有些严重偏高的。建议你参照datasheet 第12页表 8-1. Ripple Generation Methods, 可以计算反馈电路。
或者你可以借助芯片官网的在线仿真webench获得参考电路。
webench不支持LM5013设计一个48V输入,24V输出的3.5A的DC-DC电路,它总是提示我输入有问题
Hi
应该是软件bug, 如果设置成为3.2A就可以仿真出来。