This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5013: 输出电压有偏差

Part Number: LM5013


这是我设计的电路,在实际测量时,VFB=1.26V,电源纹波为三角波,VPP=200mV,频率为100K,输出电压为24.9V,输出电压为什么差0.9V,其他电压设计输出都很准,最多相差0.1V

这是什么原因造成的,图中器件都是正常的。而且用官网的电源设计软件,输入48-85V,输出24V,显示不能用LM5013设计,这是怎么回事?