This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[TPS65992]DP设备插入,发现TPS65992与外部设备无PD协议通讯,详细见正文

DEAR TI:

      我们在使用贵司(TPS65992DAE)这颗物料,遇到了棘手问题需要贵司支持!十万火急!!!

1.TPS65992DAE芯片方案背景介绍

目前我司方案:外部DP接口--》redriver器件(NB7VPQ904M )--》通过I2C连接到Pd controllerTPS65992)- -》Pd controller 通过I2C连接到ECITE8987)。

原始方案(贵司与其他厂商的默认参考方案):外部DP接口--》redriver器件(PS8802QFN52GTR-A3)--》通过I2C连接到Pd controllerTPS65992 --》Pd controller 通过I2C连接到ECITE8987)。

从上面可以看出,我司替换了原始方案的redriver这颗芯片(PS8802QFN52GTR-A3)改成了NB7VPQ904M芯片。目前我们遇到了两个问题:


1.我们替换了redriver后,发现TPS65992无法通过I2C去控制Rediver芯片(NB7VPQ904M );

问:我司替换rediver芯片后,是否需要更新TPS65992的芯片固件程序?
问:如果需要更新TPS65992的芯片固件程序,贵司是否能提供此固件程序,以匹配NB7VPQ904M呢?


2.我们替换了redriver后,发现接入外部的DP接口设备的时候,根据我们抓取图文,TPS65992并没有正确的PD协议通信报文,报文格式如下图:

问:我们想确认下,DP外设和PD控制器TPS65992之间的PD协议,是否完全由TPS65992控制?
问:如果是完全由TPS65992控制,那么上图抓取的PD协议是否正确?
问:如果上图抓取的PD协议不正确,那是由什么原因导致的的呢?需要怎么去解决呢?

3.如何能确认插入DP设备时,TPS65992的输入和输出信号是否正常?

x 出现错误。请重试或与管理员联系。