This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78Z100: 充电跳变, 放电结束跳变

Part Number: BQ78Z100
Other Parts Discussed in Thread: GPCCHEM


上图充电快结束时跳变增加 254MAH


放电结束时从198MHA直接变为0

请问这是什么原因引起的?

  • 您好,是否配置CHEM ID 并且完整学习。

  • 您好,  有配置ID  和学习,  

  • 您好,请将GPCCHEM 报告和log数发过来看一下。

  • Chemistry ID selection tool, rev=2.53		
    		
    Configuration used in present fit:		
    ProcessingType = 2		
    NumCellSeries = 2		
    ElapsedTimeColumn=2		
    VoltageColumn = 7		
    CurrentColumn = 8		
    TemperatureColumn = 6		
    		
    Best chemical ID : 2195	Best chemical ID max. deviation, % : 1.08	
    		
    		
    		
    Summary of all IDs with max. DOD deviation below 3%		
    		
    Chem ID	max DOD error, %	Max R deviation, ratio
    2195	1.08	2.85
    2892	1.1	0.43
    1302	1.1	2.49
    1565	1.11	3.32
    2489	1.17	2.58
    2304	1.23	0.64
    1944	1.25	4.96
    584	1.27	0.37
    468	1.3	1.15
    2117	1.3	1.15
    120	1.38	0.44
    1763	1.43	2.48
    3547	1.44	6.12
    2289	1.51	0.32
    1176	1.53	8.35
    194	1.54	2.47
    3721	1.55	5.64
    1304	1.57	9
    128	1.61	0.75
    161	1.62	2.81
    1124	1.62	2.81
    1452	1.62	0.41
    1328	1.63	0.74
    1296	1.65	5.76
    2290	1.66	3.11
    5754	1.67	1.3
    1221	1.67	2.05
    1185	1.69	1.86
    2022	1.69	1.75
    1375	1.71	0.49
    1344	1.72	0.49
    3329	1.72	0.1
    1362	1.72	0.48
    2316	1.73	2.84
    1649	1.75	0.09
    3853	1.76	0.87
    1343	1.76	1.33
    1345	1.79	0.48
    2232	1.79	0.1
    1923	1.79	1.71
    1347	1.8	0.07
    1288	1.81	4.08
    329	1.81	1.96
    533	1.81	3.98
    179	1.82	4.01
    1234	1.82	5.5
    1373	1.82	0.51
    1182	1.83	0.02
    116	1.84	0.36
    5727	1.84	2.8
    130	1.85	0.03
    1270	1.86	0.94
    1374	1.86	0.5
    5327	1.87	1.42
    2966	1.87	3.44
    2384	1.87	1.01
    1795	1.88	2.56
    1307	1.88	1.4
    3254	1.88	0.04
    148	1.88	0.28
    1564	1.89	2.55
    2224	1.89	0.68
    145	1.89	0.17
    1358	1.89	4.35
    1371	1.9	2.3
    2570	1.91	1.36
    189	1.91	4.21
    1535	1.91	0.28
    340	1.91	4.86
    396	1.91	1.61
    1842	1.92	1.26
    3188	1.92	2.78
    3797	1.92	3.66
    2203	1.92	2.18
    3429	1.92	6.66
    1394	1.93	3.78
    1311	1.93	1.2
    3293	1.93	3.69
    2752	1.93	0.93
    2204	1.94	3.35
    1376	1.94	3.44
    3473	1.94	0.07
    3918	1.95	1.9
    3122	1.95	2.81
    1377	1.96	2.23
    2293	1.96	0.19
    3756	1.96	0.16
    3442	1.97	0.09
    1101	1.97	1.99
    2238	1.98	1.78
    3255	1.98	2.61
    2312	1.99	1.54
    5570	1.99	1.03
    2385	1.99	1.55
    1112	2	0.28
    2209	2	2.37
    2906	2	2.79
    165	2.01	2.26
    2105	2.01	8.34
    2848	2.01	1.71
    3263	2.01	0.89
    1372	2.01	0.45
    3709	2.01	0.07
    1262	2.02	3.28
    2347	2.03	1.82
    2992	2.03	4.8
    3244	2.04	4
    1531	2.05	0.6
    3211	2.05	0.01
    1177	2.05	4.29
    372	2.05	4.17
    2339	2.05	1.61
    1289	2.05	9.62
    1327	2.05	0.34
    5211	2.05	2.41
    107	2.05	2.02
    2727	2.05	3.06
    2538	2.06	1.08
    3127	2.06	0.95
    2453	2.06	1.57
    3428	2.06	6.04
    2313	2.07	0.7
    3159	2.07	4.77
    3232	2.07	5.04
    2032	2.07	9.51
    3208	2.08	0.04
    3831	2.08	0.97
    1446	2.08	1.41
    1238	2.09	4.02
    903	2.09	4.72
    3422	2.09	5.72
    1988	2.09	0.93
    3957	2.09	1.27
    2294	2.09	0.82
    125	2.1	1.04
    3206	2.1	6.56
    1706	2.1	1.54
    389	2.1	6.31
    3469	2.1	4.16
    182	2.11	0.06
    3459	2.11	4.09
    3458	2.11	4.79
    3106	2.11	7.77
    394	2.11	4.73
    1360	2.12	2.76
    3290	2.12	7.05
    3295	2.12	7.05
    1864	2.12	0.03
    1751	2.12	2.04
    330	2.12	1.11
    1422	2.12	1.67
    3468	2.12	4.92
    3771	2.12	4.76
    144	2.12	0.24
    341	2.13	1.31
    2340	2.13	1.53
    1487	2.13	2.3
    1196	2.13	4.01
    1884	2.14	0.07
    2612	2.14	1.74
    2452	2.14	1.7
    2455	2.14	1.59
    1255	2.14	0.34
    3699	2.14	2.75
    149	2.15	0.66
    3301	2.15	2.32
    2594	2.15	1.04
    1938	2.15	1.48
    3417	2.15	1.6
    2734	2.15	3.19
    3302	2.15	4.52
    3781	2.15	3.98
    1458	2.15	2.48
    1648	2.16	0.88
    3214	2.16	0.04
    131	2.17	0.93
    363	2.17	5.15
    3432	2.17	5.88
    1368	2.18	8.66
    3731	2.18	4.67
    1620	2.18	0.54
    129	2.18	1.66
    1929	2.19	1.54
    1276	2.19	2.62
    3410	2.19	0.81
    2381	2.19	0.07
    3262	2.19	4.94
    3965	2.2	0.41
    3672	2.2	0.05
    3730	2.21	2.38
    2601	2.21	0.34
    3216	2.21	0.03
    167	2.21	4.88
    1779	2.21	0.46
    1512	2.22	1.31
    3325	2.22	5.29
    395	2.22	6.3
    5220	2.23	0.99
    512	2.23	2.33
    3690	2.23	4.43
    3502	2.24	0.05
    3545	2.24	1.1
    1197	2.24	4.65
    1188	2.24	8.22
    3752	2.24	3.47
    3506	2.25	0.01
    3927	2.25	1.54
    1359	2.25	1.75
    3351	2.26	2.05
    3858	2.26	2.09
    1260	2.26	0.03
    5349	2.26	1.08
    1209	2.26	5.5
    3347	2.27	0.54
    2378	2.27	1.33
    1504	2.27	1.09
    3854	2.27	2.7
    3407	2.27	5.44
    2184	2.27	1.2
    7012	2.28	1.71
    1378	2.28	1.14
    3441	2.29	6.78
    1266	2.29	4.47
    1872	2.29	0.68
    3605	2.29	5.09
    1207	2.29	6.14
    3143	2.29	3.62
    1283	2.29	8.78
    1829	2.29	0.48
    1497	2.29	0.96
    2819	2.3	0.56
    5995	2.3	1.57
    3448	2.3	0.11
    1865	2.3	0.82
    1426	2.31	1.8
    3521	2.31	0.62
    1811	2.31	1.11
    3354	2.31	2.3
    1701	2.31	2.05
    3472	2.31	7.08
    2337	2.31	1.55
    2013	2.32	5.74
    3794	2.32	1.33
    3217	2.32	5.89
    2422	2.32	3.24
    3673	2.33	1.68
    362	2.33	2.93
    3215	2.33	7.8
    2835	2.33	0.11
    1828	2.33	0.37
    2189	2.34	1.94
    3953	2.34	1.02
    2454	2.34	1.83
    1523	2.34	1.48
    3755	2.34	2.38
    3668	2.35	1.55
    153	2.35	0.12
    3773	2.35	3.79
    3997	2.35	1.42
    3697	2.35	1.44
    3549	2.35	0.16
    2364	2.35	2.24
    3310	2.35	0.16
    1815	2.36	0.65
    132	2.36	0.36
    3389	2.36	7.07
    3942	2.37	0.58
    1189	2.37	6.75
    3682	2.37	3.16
    3482	2.37	0.19
    2530	2.37	2.48
    1277	2.38	0.97
    2228	2.38	2.71
    2183	2.38	0.27
    3198	2.38	0.03
    3413	2.38	5.82
    1524	2.38	1.92
    3296	2.38	2.79
    1224	2.39	3.66
    1638	2.39	1.35
    133	2.39	0.3
    1421	2.39	1.65
    2729	2.39	4.12
    2288	2.39	0.09
    1856	2.39	1.35
    3835	2.39	1.72
    1232	2.39	6.5
    3925	2.4	0.22
    1677	2.4	1.35
    1906	2.4	1.47
    1403	2.41	2.32
    2169	2.41	0.01
    3930	2.41	0.08
    1776	2.41	0.19
    3451	2.41	3.69
    3535	2.41	0.17
    3707	2.41	6.17
    2950	2.41	0.96
    5113	2.41	0.87
    2382	2.42	0.18
    359	2.42	4.96
    3107	2.42	3.7
    3575	2.42	7.86
    3855	2.42	1.08
    3815	2.42	1.83
    180	2.43	0.13
    1810	2.43	0.67
    5987	2.43	2.97
    2168	2.44	1.08
    386	2.45	6.59
    3358	2.45	6.07
    2740	2.45	1.31
    2301	2.45	0.06
    506	2.46	2.45
    1250	2.46	3.38
    1639	2.46	1.13
    2652	2.46	2.12
    3667	2.46	3.7
    1557	2.47	1.07
    1285	2.47	6.63
    3446	2.48	3.87
    3553	2.48	7.12
    1562	2.48	0.87
    1511	2.48	1.88
    1911	2.48	0.69
    1924	2.48	0.36
    2722	2.48	0.11
    1777	2.48	0.01
    3885	2.48	5.57
    1820	2.49	0.89
    1628	2.49	1.53
    1566	2.49	3.76
    3663	2.49	1.4
    1907	2.49	0.88
    380	2.49	4.69
    3816	2.49	0.02
    2176	2.5	0.82
    2215	2.5	0.25
    1184	2.5	2.22
    3595	2.5	1.66
    3561	2.5	2.39
    3768	2.5	2.17
    1361	2.5	0.91
    3318	2.5	3.06
    1837	2.51	0.58
    3976	2.51	0.84
    2177	2.52	0.36
    1821	2.52	1.45
    3399	2.52	0.31
    2901	2.52	3.79
    1428	2.52	0.96
    3924	2.52	1.71
    3411	2.52	7.13
    1513	2.52	1.56
    3528	2.53	4.18
    2905	2.53	2.56
    1871	2.53	1.41
    1198	2.53	6.05
    1892	2.53	2.32
    3353	2.53	0.02
    1363	2.54	0.87
    2118	2.54	1.49
    469	2.54	1.49
    3904	2.54	1.14
    187	2.54	0.53
    1178	2.54	3.32
    1839	2.54	1.1
    1552	2.54	1.14
    1853	2.54	0.9
    1824	2.55	0.15
    1329	2.56	4.84
    1115	2.56	3.94
    3260	2.56	1.84
    1718	2.56	1.1
    3832	2.56	1.72
    3603	2.56	1.63
    1225	2.56	3.93
    2216	2.56	1.5
    3474	2.57	3.13
    1439	2.57	0.25
    2178	2.57	0.97
    3922	2.57	0.13
    3842	2.57	1.11
    3766	2.57	1.92
    2241	2.57	1.5
    3504	2.57	0.33
    1434	2.58	2.35
    3943	2.58	3.48
    1136	2.58	7.42
    1228	2.58	3.1
    2415	2.58	2.64
    1440	2.58	0.29
    1558	2.58	0.73
    1529	2.58	0.96
    2327	2.58	1.14
    1868	2.59	1.38
    3916	2.59	0
    1448	2.59	0.41
    2359	2.59	2.51
    3487	2.6	0.24
    2544	2.6	2.46
    3642	2.6	1.56
    1465	2.6	1.84
    3633	2.6	1.4
    1624	2.6	0.95
    1729	2.6	0.25
    124	2.61	1.42
    3494	2.61	1.63
    2400	2.61	1.32
    1679	2.61	1.92
    3503	2.61	4.07
    1118	2.61	2.96
    3404	2.61	5.17
    3769	2.61	1.34
    1356	2.61	0.93
    1193	2.61	5.13
    1870	2.62	1.28
    1435	2.62	0.34
    1536	2.62	1.69
    1445	2.62	0.33
    3463	2.62	2.65
    3313	2.62	6.28
    3892	2.62	1.83
    1239	2.62	0.22
    2869	2.63	1.69
    166	2.63	0.47
    1908	2.63	0.77
    1265	2.63	4.25
    3564	2.63	2.06
    109	2.64	2.27
    1888	2.64	1.24
    2596	2.64	3.84
    3888	2.64	1.4
    3964	2.64	1.52
    3366	2.65	4.2
    3982	2.66	2.25
    3848	2.66	0.02
    1444	2.66	0.32
    5836	2.66	0.05
    1195	2.66	7.31
    2310	2.66	1.99
    3611	2.67	2.2
    3631	2.67	2
    199	2.67	0.68
    1873	2.68	0.47
    3488	2.68	2.11
    1257	2.68	4.72
    3562	2.68	3.21
    1186	2.68	4.95
    1297	2.68	7.47
    3365	2.69	2.84
    3223	2.69	4.14
    2199	2.69	0.99
    2818	2.69	0.78
    1734	2.69	0.97
    1469	2.69	0.03
    1333	2.69	5.39
    1819	2.69	1.59
    1495	2.69	1.25
    1927	2.69	1.47
    3101	2.7	6.81
    5660	2.7	1.1
    3182	2.71	4.33
    3594	2.71	3.9
    2599	2.71	0.75
    379	2.71	6.38
    1699	2.71	1.34
    2451	2.72	0.44
    5116	2.72	1.85
    1438	2.72	0.38
    1582	2.73	0.71
    1317	2.73	2.8
    3464	2.73	0.33
    160	2.74	0.33
    1749	2.74	0.82
    2536	2.74	0.04
    2735	2.74	0.58
    3501	2.74	1.66
    2248	2.75	0.95
    1530	2.75	1.24
    2335	2.75	0.39
    3572	2.75	1.84
    157	2.76	0.03
    1646	2.76	0.56
    3507	2.76	2.6
    1885	2.76	1.3
    3294	2.77	6.33
    1483	2.77	1.68
    3715	2.77	3.5
    1854	2.77	1.04
    1886	2.77	1.3
    3646	2.77	1.71
    117	2.77	0.25
    3416	2.78	4.49
    3397	2.78	4.5
    2955	2.78	1.09
    3439	2.78	1.95
    3793	2.78	0.11
    2807	2.78	2.17
    2817	2.78	1.88
    1597	2.79	4.44
    1450	2.79	1.31
    3651	2.79	4.41
    1617	2.8	5.08
    1443	2.8	0.51
    1100	2.8	0.68
    2377	2.8	0.93
    5712	2.8	0.97
    1697	2.8	1.45
    1887	2.8	1.13
    3760	2.81	5.45
    2439	2.81	1
    1875	2.81	1.37
    127	2.81	1.42
    2598	2.81	0.93
    2575	2.81	0.11
    1905	2.82	1.1
    5341	2.83	2.1
    3467	2.83	2.46
    1315	2.84	3.23
    3466	2.84	2.4
    2587	2.84	0.37
    2147	2.85	4.44
    1619	2.85	1.45
    3743	2.85	2.06
    3402	2.85	2.14
    2214	2.86	0.36
    3257	2.86	3.01
    2334	2.86	0.37
    2440	2.86	0.63
    1442	2.86	0.86
    5104	2.86	0.43
    1874	2.87	1.12
    3452	2.88	0.01
    1312	2.89	1.94
    1645	2.89	1.89
    3685	2.89	0.11
    2249	2.9	0.19
    2586	2.9	0.48
    2834	2.91	2.12
    1287	2.91	1.27
    126	2.91	1.07
    2326	2.91	1.15
    1441	2.92	0.9
    1705	2.93	0.84
    1261	2.93	8.11
    2116	2.93	5.6
    467	2.93	5.6
    3519	2.93	1.17
    1326	2.93	1.17
    5185	2.94	0.42
    1720	2.94	1.4
    3691	2.94	5.9
    159	2.94	1.79
    3929	2.95	3.56
    1137	2.95	1.86
    3941	2.96	1.44
    3538	2.96	1.83
    1402	2.96	2.38
    1851	2.96	1.45
    1392	2.96	0.94
    1838	2.97	1.19
    2844	2.97	1.8
    327	2.97	1.68
    3544	2.98	1.27
    3192	2.98	1.57
    5968	2.98	1.18
    5775	2.99	0.32
    1537	2.99	5.85
    3729	2.99	4.16
    1104	2.99	0.44
    3380	3	2.78
    1704	3	2.11
    		
    Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
    		
    		
    Selection of best generic ID for ROM based devices like bq274xx		
    		
    		
    Device / Family #1		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    128	bq27421-G1A: 4.2V LiCoO2	1.61
    354	bq27411-G1C: 4.35V LiCoO2	2.68
    3142	bq27421-G1D: 4.4V LiCoO2	3.95
    312	bq27421-G1B: 4.3V LiCoO2	4.09
    Best generic ID 128		
    Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
    		
    		
    Device / Family #2		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    1202	bq27621: (default) 4.2V LiCoO2	2.61
    354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	2.68
    1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	3.2
    Best generic ID 1202		
    Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
    		
    		
    Device / Family #3		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	2.61
    3230	bq27426: (default) 4.35V LiCoO2	3.28
    3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	3.95
    Best generic ID 1202		
    Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
    		
    		
    
    3337-1.CSV

    文件已上传,  请帮忙查看一下,  非常感谢

  • 另外,  这个电池当时做数据时测试是可以的,   现在电芯搁置了几个月,  现在来生产才发现这个问题

  • 您好,正在询问更了解这款芯片的TI工程师,稍后回复。

  • 您好,One issue could be that the gauge thinks there's more capacity than there actually is. This could be due to having the CYSNC flag on, RM will jump to FCC at EOC.  

    Battery cells increase their internal resistance over time. The gauge is able to learn the resistance as it discharges, but if the cell is being seated for a long time, then the resistances might have increased and the gauge was not learning. One option is to change the load select to a mode. What is the current mode select?

    Did the customer use the GPCRA0 tool? This tool provides thermal parameters for self heating and helps predict better the load. 

    Make sure the customer has the SMOOTH feature on. Please share the setting file.



    On another thought, looking at the OCV table of the best matched ID (2195), the lowest voltage of that profile is 3V. However, the customer discharged up to 2.6V. Can you explain this?