Other Parts Discussed in Thread: GPCCHEM

上图充电快结束时跳变增加 254MAH

放电结束时从198MHA直接变为0
请问这是什么原因引起的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chemistry ID selection tool, rev=2.53 Configuration used in present fit: ProcessingType = 2 NumCellSeries = 2 ElapsedTimeColumn=2 VoltageColumn = 7 CurrentColumn = 8 TemperatureColumn = 6 Best chemical ID : 2195 Best chemical ID max. deviation, % : 1.08 Summary of all IDs with max. DOD deviation below 3% Chem ID max DOD error, % Max R deviation, ratio 2195 1.08 2.85 2892 1.1 0.43 1302 1.1 2.49 1565 1.11 3.32 2489 1.17 2.58 2304 1.23 0.64 1944 1.25 4.96 584 1.27 0.37 468 1.3 1.15 2117 1.3 1.15 120 1.38 0.44 1763 1.43 2.48 3547 1.44 6.12 2289 1.51 0.32 1176 1.53 8.35 194 1.54 2.47 3721 1.55 5.64 1304 1.57 9 128 1.61 0.75 161 1.62 2.81 1124 1.62 2.81 1452 1.62 0.41 1328 1.63 0.74 1296 1.65 5.76 2290 1.66 3.11 5754 1.67 1.3 1221 1.67 2.05 1185 1.69 1.86 2022 1.69 1.75 1375 1.71 0.49 1344 1.72 0.49 3329 1.72 0.1 1362 1.72 0.48 2316 1.73 2.84 1649 1.75 0.09 3853 1.76 0.87 1343 1.76 1.33 1345 1.79 0.48 2232 1.79 0.1 1923 1.79 1.71 1347 1.8 0.07 1288 1.81 4.08 329 1.81 1.96 533 1.81 3.98 179 1.82 4.01 1234 1.82 5.5 1373 1.82 0.51 1182 1.83 0.02 116 1.84 0.36 5727 1.84 2.8 130 1.85 0.03 1270 1.86 0.94 1374 1.86 0.5 5327 1.87 1.42 2966 1.87 3.44 2384 1.87 1.01 1795 1.88 2.56 1307 1.88 1.4 3254 1.88 0.04 148 1.88 0.28 1564 1.89 2.55 2224 1.89 0.68 145 1.89 0.17 1358 1.89 4.35 1371 1.9 2.3 2570 1.91 1.36 189 1.91 4.21 1535 1.91 0.28 340 1.91 4.86 396 1.91 1.61 1842 1.92 1.26 3188 1.92 2.78 3797 1.92 3.66 2203 1.92 2.18 3429 1.92 6.66 1394 1.93 3.78 1311 1.93 1.2 3293 1.93 3.69 2752 1.93 0.93 2204 1.94 3.35 1376 1.94 3.44 3473 1.94 0.07 3918 1.95 1.9 3122 1.95 2.81 1377 1.96 2.23 2293 1.96 0.19 3756 1.96 0.16 3442 1.97 0.09 1101 1.97 1.99 2238 1.98 1.78 3255 1.98 2.61 2312 1.99 1.54 5570 1.99 1.03 2385 1.99 1.55 1112 2 0.28 2209 2 2.37 2906 2 2.79 165 2.01 2.26 2105 2.01 8.34 2848 2.01 1.71 3263 2.01 0.89 1372 2.01 0.45 3709 2.01 0.07 1262 2.02 3.28 2347 2.03 1.82 2992 2.03 4.8 3244 2.04 4 1531 2.05 0.6 3211 2.05 0.01 1177 2.05 4.29 372 2.05 4.17 2339 2.05 1.61 1289 2.05 9.62 1327 2.05 0.34 5211 2.05 2.41 107 2.05 2.02 2727 2.05 3.06 2538 2.06 1.08 3127 2.06 0.95 2453 2.06 1.57 3428 2.06 6.04 2313 2.07 0.7 3159 2.07 4.77 3232 2.07 5.04 2032 2.07 9.51 3208 2.08 0.04 3831 2.08 0.97 1446 2.08 1.41 1238 2.09 4.02 903 2.09 4.72 3422 2.09 5.72 1988 2.09 0.93 3957 2.09 1.27 2294 2.09 0.82 125 2.1 1.04 3206 2.1 6.56 1706 2.1 1.54 389 2.1 6.31 3469 2.1 4.16 182 2.11 0.06 3459 2.11 4.09 3458 2.11 4.79 3106 2.11 7.77 394 2.11 4.73 1360 2.12 2.76 3290 2.12 7.05 3295 2.12 7.05 1864 2.12 0.03 1751 2.12 2.04 330 2.12 1.11 1422 2.12 1.67 3468 2.12 4.92 3771 2.12 4.76 144 2.12 0.24 341 2.13 1.31 2340 2.13 1.53 1487 2.13 2.3 1196 2.13 4.01 1884 2.14 0.07 2612 2.14 1.74 2452 2.14 1.7 2455 2.14 1.59 1255 2.14 0.34 3699 2.14 2.75 149 2.15 0.66 3301 2.15 2.32 2594 2.15 1.04 1938 2.15 1.48 3417 2.15 1.6 2734 2.15 3.19 3302 2.15 4.52 3781 2.15 3.98 1458 2.15 2.48 1648 2.16 0.88 3214 2.16 0.04 131 2.17 0.93 363 2.17 5.15 3432 2.17 5.88 1368 2.18 8.66 3731 2.18 4.67 1620 2.18 0.54 129 2.18 1.66 1929 2.19 1.54 1276 2.19 2.62 3410 2.19 0.81 2381 2.19 0.07 3262 2.19 4.94 3965 2.2 0.41 3672 2.2 0.05 3730 2.21 2.38 2601 2.21 0.34 3216 2.21 0.03 167 2.21 4.88 1779 2.21 0.46 1512 2.22 1.31 3325 2.22 5.29 395 2.22 6.3 5220 2.23 0.99 512 2.23 2.33 3690 2.23 4.43 3502 2.24 0.05 3545 2.24 1.1 1197 2.24 4.65 1188 2.24 8.22 3752 2.24 3.47 3506 2.25 0.01 3927 2.25 1.54 1359 2.25 1.75 3351 2.26 2.05 3858 2.26 2.09 1260 2.26 0.03 5349 2.26 1.08 1209 2.26 5.5 3347 2.27 0.54 2378 2.27 1.33 1504 2.27 1.09 3854 2.27 2.7 3407 2.27 5.44 2184 2.27 1.2 7012 2.28 1.71 1378 2.28 1.14 3441 2.29 6.78 1266 2.29 4.47 1872 2.29 0.68 3605 2.29 5.09 1207 2.29 6.14 3143 2.29 3.62 1283 2.29 8.78 1829 2.29 0.48 1497 2.29 0.96 2819 2.3 0.56 5995 2.3 1.57 3448 2.3 0.11 1865 2.3 0.82 1426 2.31 1.8 3521 2.31 0.62 1811 2.31 1.11 3354 2.31 2.3 1701 2.31 2.05 3472 2.31 7.08 2337 2.31 1.55 2013 2.32 5.74 3794 2.32 1.33 3217 2.32 5.89 2422 2.32 3.24 3673 2.33 1.68 362 2.33 2.93 3215 2.33 7.8 2835 2.33 0.11 1828 2.33 0.37 2189 2.34 1.94 3953 2.34 1.02 2454 2.34 1.83 1523 2.34 1.48 3755 2.34 2.38 3668 2.35 1.55 153 2.35 0.12 3773 2.35 3.79 3997 2.35 1.42 3697 2.35 1.44 3549 2.35 0.16 2364 2.35 2.24 3310 2.35 0.16 1815 2.36 0.65 132 2.36 0.36 3389 2.36 7.07 3942 2.37 0.58 1189 2.37 6.75 3682 2.37 3.16 3482 2.37 0.19 2530 2.37 2.48 1277 2.38 0.97 2228 2.38 2.71 2183 2.38 0.27 3198 2.38 0.03 3413 2.38 5.82 1524 2.38 1.92 3296 2.38 2.79 1224 2.39 3.66 1638 2.39 1.35 133 2.39 0.3 1421 2.39 1.65 2729 2.39 4.12 2288 2.39 0.09 1856 2.39 1.35 3835 2.39 1.72 1232 2.39 6.5 3925 2.4 0.22 1677 2.4 1.35 1906 2.4 1.47 1403 2.41 2.32 2169 2.41 0.01 3930 2.41 0.08 1776 2.41 0.19 3451 2.41 3.69 3535 2.41 0.17 3707 2.41 6.17 2950 2.41 0.96 5113 2.41 0.87 2382 2.42 0.18 359 2.42 4.96 3107 2.42 3.7 3575 2.42 7.86 3855 2.42 1.08 3815 2.42 1.83 180 2.43 0.13 1810 2.43 0.67 5987 2.43 2.97 2168 2.44 1.08 386 2.45 6.59 3358 2.45 6.07 2740 2.45 1.31 2301 2.45 0.06 506 2.46 2.45 1250 2.46 3.38 1639 2.46 1.13 2652 2.46 2.12 3667 2.46 3.7 1557 2.47 1.07 1285 2.47 6.63 3446 2.48 3.87 3553 2.48 7.12 1562 2.48 0.87 1511 2.48 1.88 1911 2.48 0.69 1924 2.48 0.36 2722 2.48 0.11 1777 2.48 0.01 3885 2.48 5.57 1820 2.49 0.89 1628 2.49 1.53 1566 2.49 3.76 3663 2.49 1.4 1907 2.49 0.88 380 2.49 4.69 3816 2.49 0.02 2176 2.5 0.82 2215 2.5 0.25 1184 2.5 2.22 3595 2.5 1.66 3561 2.5 2.39 3768 2.5 2.17 1361 2.5 0.91 3318 2.5 3.06 1837 2.51 0.58 3976 2.51 0.84 2177 2.52 0.36 1821 2.52 1.45 3399 2.52 0.31 2901 2.52 3.79 1428 2.52 0.96 3924 2.52 1.71 3411 2.52 7.13 1513 2.52 1.56 3528 2.53 4.18 2905 2.53 2.56 1871 2.53 1.41 1198 2.53 6.05 1892 2.53 2.32 3353 2.53 0.02 1363 2.54 0.87 2118 2.54 1.49 469 2.54 1.49 3904 2.54 1.14 187 2.54 0.53 1178 2.54 3.32 1839 2.54 1.1 1552 2.54 1.14 1853 2.54 0.9 1824 2.55 0.15 1329 2.56 4.84 1115 2.56 3.94 3260 2.56 1.84 1718 2.56 1.1 3832 2.56 1.72 3603 2.56 1.63 1225 2.56 3.93 2216 2.56 1.5 3474 2.57 3.13 1439 2.57 0.25 2178 2.57 0.97 3922 2.57 0.13 3842 2.57 1.11 3766 2.57 1.92 2241 2.57 1.5 3504 2.57 0.33 1434 2.58 2.35 3943 2.58 3.48 1136 2.58 7.42 1228 2.58 3.1 2415 2.58 2.64 1440 2.58 0.29 1558 2.58 0.73 1529 2.58 0.96 2327 2.58 1.14 1868 2.59 1.38 3916 2.59 0 1448 2.59 0.41 2359 2.59 2.51 3487 2.6 0.24 2544 2.6 2.46 3642 2.6 1.56 1465 2.6 1.84 3633 2.6 1.4 1624 2.6 0.95 1729 2.6 0.25 124 2.61 1.42 3494 2.61 1.63 2400 2.61 1.32 1679 2.61 1.92 3503 2.61 4.07 1118 2.61 2.96 3404 2.61 5.17 3769 2.61 1.34 1356 2.61 0.93 1193 2.61 5.13 1870 2.62 1.28 1435 2.62 0.34 1536 2.62 1.69 1445 2.62 0.33 3463 2.62 2.65 3313 2.62 6.28 3892 2.62 1.83 1239 2.62 0.22 2869 2.63 1.69 166 2.63 0.47 1908 2.63 0.77 1265 2.63 4.25 3564 2.63 2.06 109 2.64 2.27 1888 2.64 1.24 2596 2.64 3.84 3888 2.64 1.4 3964 2.64 1.52 3366 2.65 4.2 3982 2.66 2.25 3848 2.66 0.02 1444 2.66 0.32 5836 2.66 0.05 1195 2.66 7.31 2310 2.66 1.99 3611 2.67 2.2 3631 2.67 2 199 2.67 0.68 1873 2.68 0.47 3488 2.68 2.11 1257 2.68 4.72 3562 2.68 3.21 1186 2.68 4.95 1297 2.68 7.47 3365 2.69 2.84 3223 2.69 4.14 2199 2.69 0.99 2818 2.69 0.78 1734 2.69 0.97 1469 2.69 0.03 1333 2.69 5.39 1819 2.69 1.59 1495 2.69 1.25 1927 2.69 1.47 3101 2.7 6.81 5660 2.7 1.1 3182 2.71 4.33 3594 2.71 3.9 2599 2.71 0.75 379 2.71 6.38 1699 2.71 1.34 2451 2.72 0.44 5116 2.72 1.85 1438 2.72 0.38 1582 2.73 0.71 1317 2.73 2.8 3464 2.73 0.33 160 2.74 0.33 1749 2.74 0.82 2536 2.74 0.04 2735 2.74 0.58 3501 2.74 1.66 2248 2.75 0.95 1530 2.75 1.24 2335 2.75 0.39 3572 2.75 1.84 157 2.76 0.03 1646 2.76 0.56 3507 2.76 2.6 1885 2.76 1.3 3294 2.77 6.33 1483 2.77 1.68 3715 2.77 3.5 1854 2.77 1.04 1886 2.77 1.3 3646 2.77 1.71 117 2.77 0.25 3416 2.78 4.49 3397 2.78 4.5 2955 2.78 1.09 3439 2.78 1.95 3793 2.78 0.11 2807 2.78 2.17 2817 2.78 1.88 1597 2.79 4.44 1450 2.79 1.31 3651 2.79 4.41 1617 2.8 5.08 1443 2.8 0.51 1100 2.8 0.68 2377 2.8 0.93 5712 2.8 0.97 1697 2.8 1.45 1887 2.8 1.13 3760 2.81 5.45 2439 2.81 1 1875 2.81 1.37 127 2.81 1.42 2598 2.81 0.93 2575 2.81 0.11 1905 2.82 1.1 5341 2.83 2.1 3467 2.83 2.46 1315 2.84 3.23 3466 2.84 2.4 2587 2.84 0.37 2147 2.85 4.44 1619 2.85 1.45 3743 2.85 2.06 3402 2.85 2.14 2214 2.86 0.36 3257 2.86 3.01 2334 2.86 0.37 2440 2.86 0.63 1442 2.86 0.86 5104 2.86 0.43 1874 2.87 1.12 3452 2.88 0.01 1312 2.89 1.94 1645 2.89 1.89 3685 2.89 0.11 2249 2.9 0.19 2586 2.9 0.48 2834 2.91 2.12 1287 2.91 1.27 126 2.91 1.07 2326 2.91 1.15 1441 2.92 0.9 1705 2.93 0.84 1261 2.93 8.11 2116 2.93 5.6 467 2.93 5.6 3519 2.93 1.17 1326 2.93 1.17 5185 2.94 0.42 1720 2.94 1.4 3691 2.94 5.9 159 2.94 1.79 3929 2.95 3.56 1137 2.95 1.86 3941 2.96 1.44 3538 2.96 1.83 1402 2.96 2.38 1851 2.96 1.45 1392 2.96 0.94 1838 2.97 1.19 2844 2.97 1.8 327 2.97 1.68 3544 2.98 1.27 3192 2.98 1.57 5968 2.98 1.18 5775 2.99 0.32 1537 2.99 5.85 3729 2.99 4.16 1104 2.99 0.44 3380 3 2.78 1704 3 2.11 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 128 bq27421-G1A: 4.2V LiCoO2 1.61 354 bq27411-G1C: 4.35V LiCoO2 2.68 3142 bq27421-G1D: 4.4V LiCoO2 3.95 312 bq27421-G1B: 4.3V LiCoO2 4.09 Best generic ID 128 Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family. Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 1202 bq27621: (default) 4.2V LiCoO2 2.61 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 2.68 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 3.2 Best generic ID 1202 Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family. Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 2.61 3230 bq27426: (default) 4.35V LiCoO2 3.28 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 3.95 Best generic ID 1202 Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.
文件已上传, 请帮忙查看一下, 非常感谢
您好,One issue could be that the gauge thinks there's more capacity than there actually is. This could be due to having the CYSNC flag on, RM will jump to FCC at EOC.
Battery cells increase their internal resistance over time. The gauge is able to learn the resistance as it discharges, but if the cell is being seated for a long time, then the resistances might have increased and the gauge was not learning. One option is to change the load select to a mode. What is the current mode select?
Did the customer use the GPCRA0 tool? This tool provides thermal parameters for self heating and helps predict better the load.
Make sure the customer has the SMOOTH feature on. Please share the setting file.
On another thought, looking at the OCV table of the best matched ID (2195), the lowest voltage of that profile is 3V. However, the customer discharged up to 2.6V. Can you explain this?