This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Original question:
[参考译文] LM7400-Q1:LM7400-Q1和 lm74722-Q1
Part Number: LM74720-Q1
单芯片怎么增加电流呢?
Hi
可以做到5A的。
感谢工程师的回答,是这样的,我需要做到50A,甚至更多,这款芯片能满足吗?如果能满足我将修改哪些方面?我用100V300A的mos替换Q2,在使用en使能热插拔负载时,5A电流时正常,但10A时会烧毁Q2,以及LM74720芯片.我不知道什么是那些参数影响了他?
电流足够大,需要更大电流的MOS, 甚至要MOS并联。我这边没有看到这么大电流的方案,但是应该是可以的。