使用BQ24073给单节18650电池充电,如果电池正负极接反了,会怎么样?BQ24073是否具备防反功能触发保护,还是会烧毁?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The BQ24073 does not have a reverse polarity protection built into the device. Take a look at this app note which discusses how to do this with the TPS27051A switch. www.ti.com/.../slva798.pdf
您好,没有找到适合这款芯片的负载反接电路。
The BQ24073 device features Input-bassed dynamic power management (Vin-DPM), 28-V Input rating with OVP, Integrated Dynamic Power Path Management (DPPM), Reverse current protection, short-circuit protection, and thermal protection.
For voltage at the input, the absolute maximum rating is from -0.3 to 28V. Stresses beyond this voltage may cause permanent damage to the device.