This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520: 计算拉电流公式怎么来的,不是特别明白

Part Number: UCC21520


 UCC21520数据手册里面9.2节计算电流出现了这个公式。但是对于这个公式怎么来的不是很明白,可以具体详细解释一下吗

  • Hi

        解释第二个公式驱动放电电路,VDD-Vgdf是驱动电压减去驱动MOS压降,Rol+Roff//Ron+Rgfet_int  放电回路的阻抗,Rol是芯片内部驱动电阻的导通阻抗,Ron//Roff是驱动电阻,Rgfet_int 是外部MOS G极阻抗。

        同样第一个公式是高边驱动放电电路。

  • 手册里面说是VGDF是The anti-parallel diode forward voltage drop which is in series with ROFF,RGFET_INT是Power transistor internal gate resistance,这个那一个说法是正确的呢,另外这里说的驱动电压是指芯片引脚的电压吗

     可以按照这个图说一下吗

  • Hi

        不看这个图,看图第20页图9-2,路径从VDD到Vout, 然后经过驱动电阻RON,  最后到MOS.  电流计算就是,VDD-Vgdf/(Rol+Roff//Ron+Rgfet_int )