1.目前正在调试BQ4050,对于电压校准可以顺利进行,但是在进行电流校准的时候我是用的放电的方式,外接放电设备,设置的是1A电流放电,我是先开始放电,然后软件里设置的是-1000ma,一点击校准,软件就会关闭,放电也会停止,PCB上应该是关断了。请问这个情况有可能是什么引起的。
2.我现在调试BQ4050,我的设计要求是,LED在芯片正常状态是常亮来显示电量的,如果芯片检测到没有输入输出电流时,经过设置的时间进入sleep模式。此时LED也灭,然后再放电或者充电使得芯片激活以后,LED再常亮或者闪烁。(1)进入SLEEP模式以后,要实现可以通过充放电唤醒芯片,FET要保持常开还是关闭也可以?
(2)LED灯怎么跟随Sleep模式,进入Sleep模式以后就关闭,芯片唤醒以后就常亮,充电闪烁,,,,,,现在还有个问题是现在没有充放电,但是LED有一个灯一直会闪烁不知道是什么原因
(3)芯片进入Sleep模式的时候,我只需要保留哪些功能既能保证功耗最小,也能保证可以通过充放电唤醒芯片