1、有什么情况会导致UCC28740的HV引脚失效 使得芯片不能启动?
2、有什么情况会导致UCC28740的DRV引脚和GND引脚短路?
3、推荐焊接UCC28740的温度是多少?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、有什么情况会导致UCC28740的HV引脚失效 使得芯片不能启动?
2、有什么情况会导致UCC28740的DRV引脚和GND引脚短路?
3、推荐焊接UCC28740的温度是多少?
谢谢
Hi
1. 测试一下HV脚阻抗是否较低? HV 700V耐压,一般来说很难烧掉的。
2. 确认一下VDD也损坏了? 或者驱动MOS是否烧掉,这样也很容烧驱动。
3. 手焊温度350℃+/-10℃, 如果是reflow查看焊接等级(一般不会最高不会超过245℃)