This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: HV引脚 失效无法启动 DRV引脚和GND引脚短路 推荐焊接温度

Part Number: UCC28740


1、有什么情况会导致UCC28740的HV引脚失效 使得芯片不能启动?

2、有什么情况会导致UCC28740的DRV引脚和GND引脚短路?

3、推荐焊接UCC28740的温度是多少?

谢谢

  • Hi

        1. 测试一下HV脚阻抗是否较低? HV 700V耐压,一般来说很难烧掉的。

        2.  确认一下VDD也损坏了? 或者驱动MOS是否烧掉,这样也很容烧驱动。

        3. 手焊温度350℃+/-10℃, 如果是reflow查看焊接等级(一般不会最高不会超过245℃)