This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40Z80的PRES/ SHUTDN/ DISP/ PDSG/GPIO脚是否可以设置成shutdown模式,实现shutdown和wakeup的功能

Part Number: BQ40Z80


Hi There,

BQ40Z80的TRM中有提到PIN17可以设置成shutdown,或者exit shutdown模式。关于这个功能我有一些问题。

1. 用/Shutdown PIn控制的shutdown,叫做紧急shutdown。紧急shutdown的电流是否和普通shutdown的静态电流一样?普通shutdown的电流的典型值是1.4uA.

2. TRM提到当BMS正常工作时,在/shutdown脚,如果收到一个从高电平到低电平的变化,BMS会紧急shutdown。在紧急shutdown模式,如果收到一个从高电平到低电平的变化,BMS会exit shutdown。不知道我理解是否正确?

3. 要在/shutdown脚上,实现从高电平向低电平转换,需要有一个按键一端接地,另外一端连接到Vbattery. (我是7串的电池,最高电压30V). 是否BMS的/shutdown可以设置成上拉?还是必须外接上拉电阻。如果上拉电阻是10K,会有多少的耗电流?

Regards

Alex Chen