Other Parts Discussed in Thread: BQ500412
请参考如下原理图,帮忙提出改进意见和建议
1.无线充电芯片PIN5和PIN16出现对地短路现象,失效率0.1%左右
2.请帮忙验证原理图设计是否有问题,有尝试在5、16脚串联10Ω电阻,效果并不好
3.为了排除可能存在的输入高压脉冲,尝试了并联TVS,效果也不是很好

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请参考如下原理图,帮忙提出改进意见和建议
1.无线充电芯片PIN5和PIN16出现对地短路现象,失效率0.1%左右
2.请帮忙验证原理图设计是否有问题,有尝试在5、16脚串联10Ω电阻,效果并不好
3.为了排除可能存在的输入高压脉冲,尝试了并联TVS,效果也不是很好

您好,A short on Clamp 1 and Clamp 2 is indicating an over voltage condition on the input.
The circuit looks OK
Couple of things:
1.) Send data sheet on the coil for review
2.) Check voltage rating on capacitors on AC side, should be min of 25V.
3.) When does the fail occur?
Moving the RX from a weak coupling position to a good position will cause a voltage spike on input and possible damage.
Part 4 Reference Designs_V1.2.4-A13.pdf
please help refer question 1
您好,请参考下面内容:
The Coil looks OK.
How much load in on the Coil, 250mA to 500mA?
CLAMP 1 / 2 are often active when the device is moved from a Poor coupling position to a Good coupling position. The AC 1 / 2 signal will go from normal to very high.
Have the fails been seen during device movement?