This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013B-Q1: 出现CLAMP1和CLAMP2脚对地短路问题

Part Number: BQ51013B-Q1
Other Parts Discussed in Thread: BQ500412

请参考如下原理图,帮忙提出改进意见和建议

1.无线充电芯片PIN5和PIN16出现对地短路现象,失效率0.1%左右

2.请帮忙验证原理图设计是否有问题,有尝试在5、16脚串联10Ω电阻,效果并不好

3.为了排除可能存在的输入高压脉冲,尝试了并联TVS,效果也不是很好