This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: BQ4050进行设计并使用4个 LED的问题

Part Number: BQ4050


我采用 BQ4050进行设计并使用4个 LED、 LED CHG THRESH1为0%,CHG THRESH2 为25%,CHG THRESH3为50%,CHG THRESH4为75%,CHG THRESH5为100%。

在充电测试期间、LED 显示正常。 当 RSOC 达到100%时、LED2和 LED4将闪烁、LED1和 LED3始终开启且正常。 在使用5个 LED 指示灯进行测试时没有此类问题。

LED设置成100%,问题还是一样.

如何关闭  LED2和 LED4问闪烁问题?