芯片型号:TPS659102
按照DataSheet参考设计PCB,芯片其他输出通道输出正常,只有VIO不能输出默认的1.8V的电压,而实际输出电压为3.2V,不知道这是什么原因?
设计原理图如下:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,这些电压都需要通过软件设置。首先找到相关电压的寄存器,然后根据产品说明书的设置改写寄存器。举例:比如需要设置VIO=1.8v, 首先找到该寄存器地址为0x20,里面的内容为8位,其中高6,7位是设置最大输出电流,4,5位保留,2,3位也就是前面提到的SEL设置为01,时,VIO输出就为1.8V。0,1位表示该电源ON/OFF,设置为01是ON。其它几个电源依此类推,都需要通过对相应的寄存器进行设置,请详细阅读我们的说明书,并和你们的软件工程师配合完成。
Curly Li: 我现在处于硬件PCB调试阶段,这个PMIC电压输出不对,整个硬件系统都起不来,自然不能通过软件设置相应的寄存器。PCB设计参考TPS659102 User Guide for S3C6410这个文档,上面标示VIO默认输出为1.8V,我就想知道TPS659102这款芯片PWRON启动后VIO端口是否默认应该输出为1.8V?TI官方给出的TPS659102 User Guide for S3C6410这个手册是否正确?硬件怎样连接才能让VIO默认输出1.8V?万分感谢!