This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: VIN=12V, Io=3A的时候会出现次谐波震荡

Part Number: LM5176

在使用LM5176这个料设计一款输入VIN=6~36V,输出12V/3A的电源,Fsw=300kHz。在输入电压VIN=6~11V以及VIN=13~36V带载输出均正常,但是在VIN=12V的时候,SW波形有大小波现象:

Comp补偿引脚的电阻电容以及Cslope是按照ti提供的 LM5176 Quick Start tool excel计算表格里面推荐的数值。

请问:这个现象是什么原因呢?