This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116遇到新问题!过载保护后断电空载只输出3.7V,LM5116彻底坏了吗?能恢复12V正常输出吗?

Other Parts Discussed in Thread: LM5116

12V电源板,电感15UH ,频率300KH,最大电流3.7A保护,空载输出12.21V正常,带4R输出9V出现保护(此时电流3A不应该保护),几秒钟就降到几乎接近0V,立刻切断供电,空载后输出3.7V,空载已经不能再恢复12V。请问这种情况说明LM5116已经彻底坏了吗?如果没坏,怎样调整电路恢复正常输出呢?我设计的是两层电路板,请在PCB上也提出修改意见。

此LM5116有些脚电压值和正常时没有变化,但有些管脚已和正常值有变化,有变化的管脚是:

LM5116第7脚ss是0.5V;

LM5116第8脚SB是0.38V;

LM5116第9脚COMP是4.8V;

LM5116第11脚DEMB是0.43V;

LM5116第16脚VCC是5.11V;

LM5116第18脚HB是4.67V;

LM5116第20脚SW是3.9V;

LM5116第3脚SYNC是300KHZ的毛刺,300mVp-p,正常时的方波已经没有;

LM5116第15脚LO是300KHZ的脉冲,5Vp-p,正常时的方波已经没有;

LM5116第19脚HO是300KHZ的毛刺,10Vp-p,正常时的方波已经没有;

请问这种情况说明LM5116已经彻底坏了吗?如果没坏,怎样恢复正常输出呢?请高手指教,谢谢!!

12V电源板PCB文件.rar
  • Hi!亲;你的PCB没改啊!还是水泥电阻!这。。。这你就是换100个马甲;神仙也帮不了你啊!!!!

    过载————负压————IC拴锁,就是这么个逻辑过程,信不信由你,东西就是这样。

  • 我准备马上修改PCB,但是目前遇到的这种情况,是PCB干扰太大造成的吗?我这是两层PCB,请问下步怎样修改PCB?请指出具体修改细节,目前很多片LM5116都遇到上面这种情况,请给出具体修改步骤,谢谢!

  • 亲;现在你的板上有这么几个问题。

    1)电流取样用贴片电阻。

    2)建议MOSFET换成SO-8或IPAK等小型表帖封装。这些封装已经足够支持这个电流了。选管时;不要光看电流;需要算一下功耗。

    3)开关半桥根前加贴片退耦电容,建议用1206封装 105以上的电容。X5Z、X7R的都可以。

    4)功率线用开尔文法布线。不要随意大面积覆铜。

    5)如有可能;功率电感选用带屏蔽的结构。