12V电源板,电感15UH ,频率300KH,最大电流3.7A保护,空载输出12.21V正常,带4R输出9V出现保护(此时电流3A不应该保护),几秒钟就降到几乎接近0V,立刻切断供电,空载后输出3.7V,空载已经不能再恢复12V。请问这种情况说明LM5116已经彻底坏了吗?如果没坏,怎样调整电路恢复正常输出呢?我设计的是两层电路板,请在PCB上也提出修改意见。
此LM5116有些脚电压值和正常时没有变化,但有些管脚已和正常值有变化,有变化的管脚是:
LM5116第7脚ss是0.5V;
LM5116第8脚SB是0.38V;
LM5116第9脚COMP是4.8V;
LM5116第11脚DEMB是0.43V;
LM5116第16脚VCC是5.11V;
LM5116第18脚HB是4.67V;
LM5116第20脚SW是3.9V;
LM5116第3脚SYNC是300KHZ的毛刺,300mVp-p,正常时的方波已经没有;
LM5116第15脚LO是300KHZ的脉冲,5Vp-p,正常时的方波已经没有;
LM5116第19脚HO是300KHZ的毛刺,10Vp-p,正常时的方波已经没有;
请问这种情况说明LM5116已经彻底坏了吗?如果没坏,怎样恢复正常输出呢?请高手指教,谢谢!!