This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28063: UCC28063高压输入时带载启动异常

Part Number: UCC28063


请教一问题,目前我用28063调试一台1000W的PFC 输入电压在100-277V PFC电压440V  效率0.976,现遇到一个问题有几点
1、在高于260V输入时开机FC电压无法正常起来,在260V以下开机能正常带载起机,输入调到高到277V均正常
2、输入电压超过280V时PFC开始出现异常,只有当电压降低至255 V以下又恢复正常